When I use the Timer mode ,I don't know why the callback function always running! I use the Function vAHI_TimerEnable() to configure the timer1 ,and use vAHI_TimerStartSingleShot() to start the timer .
Relative detail can be seen fowlling:
Thanks for your help!
解決済! 解決策の投稿を見る。
Hi,
You need to clear the interrupt flag.
SwVectTable
.globl PIC_SwVectTable
.
.
.extern vISR_Timer0
.
Also, you must include the u8AHI_TimerFired API to clear the interrupt flag.
(void) u8AHI_TimerFired(E_AHI_TIMER_0);
Regards,
Mario
Hi,
You need to clear the interrupt flag.
SwVectTable
.globl PIC_SwVectTable
.
.
.extern vISR_Timer0
.
Also, you must include the u8AHI_TimerFired API to clear the interrupt flag.
(void) u8AHI_TimerFired(E_AHI_TIMER_0);
Regards,
Mario
Hi,Mario
I am a beginner, Can I ask a question? I will be very grateful.
That is, must I set the interrupt priority level with the function vAHI_InterruptSetPriority()?
Look forward to your reply!
hs
Hi,
Look at the irq_JN516x.S the PIC_ChannelPriorities and PIC_SwVectTable. You can define the priority there.
Regards,
Mario
Hi, Mario
I have already set it up in the .S file (irq_JN516x.S), however,if there is no the function vAHI_InterruptSetPriority(), it can not enter the callback function, can you tell me where is wrong? Thank you!
Regards,
hs
Hi,
Please see the code below. look at the Timer 0
PIC_ChannelPriorities:
.byte 0 # pwm1 priority
.byte 0 # pwm2 priority
.byte 15 # system controller priority
.byte 7 # MAC priority
.byte 0 # AES priority
.byte 0 # PHY priority
.byte 0 # uart0 priority
.byte 0 # uart1 priority
.byte 5 # timer0 priority
.byte 0 # spi slave priority
.byte 0 # i2c maste/slave priority
.byte 0 # spi master priority
.byte 13 # pwm4 priority
.byte 0 # analog peripherals priority
.byte 14 # pwm3 priority
.byte 12 # tick timer priority
.globl PIC_SwVectTable
.section .text,"ax"
.extern zps_isrMAC
.extern ISR_vTickTimer
.extern vISR_Timer3
.extern vISR_Timer4
.extern vISR_SystemController
.align 4
.type PIC_SwVectTable, @object
.size PIC_SwVectTable, 64
PIC_SwVectTable:
.word vUnclaimedInterrupt # 0
.word vUnclaimedInterrupt # 1
.word vUnclaimedInterrupt # 2
.word vUnclaimedInterrupt # 3
.word vUnclaimedInterrupt # 4
.word APP_isrTimer0 # 5
.word vUnclaimedInterrupt # 6
.word zps_isrMAC # 7
.word vUnclaimedInterrupt # 8
.word vUnclaimedInterrupt # 9
.word vUnclaimedInterrupt # 10
.word vUnclaimedInterrupt # 11
.word ISR_vTickTimer # 12
.word vISR_Timer4 # 13
.word vISR_Timer3 # 14
.word vISR_SystemController # 15
Regards,
Mario
Hi,Mario
This is the .S file on my side, I have already followed the settings you said. But, It still can not enter the callback function if the function vAHI_InterruptSetPriority() is not used. ( I based on JN-AN-1217-ZigBee 3.0-Base-Device)
.globl PIC_ChannelPriorities
.section .text,"ax"
.align 4
.type PIC_ChannelPriorities, @object
.size PIC_ChannelPriorities, 16
PIC_ChannelPriorities:
.byte 0 # pwm1 priority
.byte 0 # pwm2 priority
.byte 15 # system controller priority
.byte 7 # MAC priority
.byte 0 # AES priority
.byte 0 # PHY priority
.byte 0 # uart0 priority
.byte 0 # uart1 priority
.byte 5 # timer0 priority
.byte 0 # spi slave priority
.byte 0 # i2c maste/slave priority
.byte 0 # spi master priority
.byte 0 # pwm4 priority
.byte 0 # analog peripherals priority
.byte 0 # pwm3 priority
.byte 12 # tick timer priority
.globl PIC_SwVectTable
.section .text,"ax"
.extern zps_isrMAC
.extern ISR_vTickTimer
.extern vISR_Timer3
.extern vISR_Timer4
.extern vISR_SystemController.align 4
.type PIC_SwVectTable, @object
.size PIC_SwVectTable, 64
PIC_SwVectTable:
.word vUnclaimedInterrupt # 0
.word vUnclaimedInterrupt # 1
.word vUnclaimedInterrupt # 2
.word vUnclaimedInterrupt # 3
.word vUnclaimedInterrupt # 4
.word Timer1_callback # 5
.word vUnclaimedInterrupt # 6
.word zps_isrMAC # 7
.word vUnclaimedInterrupt # 8
.word vUnclaimedInterrupt # 9
.word vUnclaimedInterrupt # 10
.word vUnclaimedInterrupt # 11
.word ISR_vTickTimer # 12
.word vUnclaimedInterrupt # 13
.word vUnclaimedInterrupt # 14
.word vISR_SystemController # 15
Thanks.
Regards,
hs
Hi,
Just to confirm, you want a timer and enter to the callback and make a routine. Am I correct?
Why are you trying to call vAHI_InterruptSetPriority API?
Regards,
Mario
Hi,Mario
Yes, Use timer timing and generate interrupts, If I do not use this function vAHI_InterruptSetPriority API, it will not be able to respond normally to the interrupt generated by the timer -- that is, cannot enter the callback function. So,I just want to know, is this function vAHI_InterruptSetPriority necessary for interrupts? The manual is not very detailed, I am a bit confused. The following is my code.
PUBLIC void Timer_Init()
{
vAHI_TimerEnable(E_AHI_TIMER_1,10,FALSE,TRUE,TRUE);//timer1,Low-2-High
vAHI_TimerConfigureOutputs(E_AHI_TIMER_1,FALSE,TRUE);
vAHI_TimerStartRepeat(E_AHI_TIMER_1,7813,15625);//1s //101
vAHI_Timer1RegisterCallback(Timer1_callback);
//vAHI_InterruptSetPriority(MICRO_ISR_MASK_TMR1,5);
DBG_vPrintf(TRUE, "\n\nTimer_Init()... .\n");
}
PUBLIC void Timer1_callback(uint32 u32DeviceId,uint32 u32ItemBitmap)
{
(void)u8AHI_TimerFired(E_AHI_TIMER_1);//clear interrupt flag
DBG_vPrintf(TRUE, "\n.Timer1 Interrupt handling.... .\n");
}
Tanks!
Regards,
hs
Hi,
Could you please look at the next community post?
https://community.nxp.com/thread/506029
Regards,
Mario
Hi,Mario
I will do that,Thanks!
Regards,
hs
Hi,Mario
It works! Thank you very much!