Raspberry Pi 2 Model B, Host Firmware won't Run

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Raspberry Pi 2 Model B, Host Firmware won't Run

1,722件の閲覧回数
lyncheese
Contributor I


Hello,

Recently, I just purchased JN5168 Modules, in my plan It will become IoT nodes for my project.

Right now, I'm trying to create the Gateway Host using Raspberry 2 Model B+.

I have downloaded the image, "openwrt-brcm2708-sdcard-vfat-ext4.img" and burn it to microSD 8GB,

using the Win32DiskImager.

After that, I plugged it to the Pi.

But, nothing is going on. The Green LED just lit on at first for a while and then It turned off.

The Ethernet Led also didn't turn on at all.

Anybody ever have the same problem ?

I don't know where is my mistake.

Thank you.

Warms regards.

ラベル(2)
タグ(3)
0 件の賞賛
返信
0 返答(返信)