RW612 EAPOL 4-Way Handshake delay

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

RW612 EAPOL 4-Way Handshake delay

1,513件の閲覧回数
johnny_h
Contributor I

Dear community, I’m currently working on the Wi-Fi settings for RW612. I’ve noticed a significant delay in the four-way handshake process. As shown below, RW612 takes approximately 45 milliseconds to send M2 back to the AP. Usually, it should be less than 10 milliseconds. This delay could potentially impact the efficiency of roaming.

What could be the potential causes for this extended response time? Thanks.

I am running the test on SDK 24_12_00 with wifi_wpa_supplicant example.

 

6986 7.657287   AP_mac          RW612_mac   EAPOL 193 Key (Message 1 of 4)

7027 7.7031460   RW612_mac   AP_mac          EAPOL 193 Key (Message 2 of 4)

7029 7.705378    AP_mac          RW612_mac   EAPOL 227 Key (Message 3 of 4)

7031 7.708615      RW612_mac   AP_mac          EAPOL 171 Key (Message 4 of 4)

 

0 件の賞賛
返信
3 返答(返信)

1,401件の閲覧回数
gil_simsic
NXP Employee
NXP Employee

Hello Johnny,

Please see below. It takes a fraction of a second between the messages. 

Below is an attempt i have just done...

Questions

(1) do you have any sniffer log to show if there was any re-tries?

(2) Did you make any changes to the example? Which AP are you using? How did you set the RW612 as a STA (what is the command line info)

(3) Please look into UM11797 NXP Wi-Fi and Bluetooth Debug Feature Configuration for
RW61x Evaluation Board. p 4. If possible, can you enable some of the debug?

(4) at your earliest convenience, please share with us 

- OTA (over the air) sniffer log

- full terminal log 

 

Thank you!

 

gil_simsic_0-1743768719207.png

 

Gil Simsic
Wireless FAE
NXP
0 件の賞賛
返信

1,482件の閲覧回数
ctnxp
NXP Employee
NXP Employee

Hi Johnny, 

Our team is reviewing this and will get back to you soon. 

-Cynthia 

0 件の賞賛
返信

1,485件の閲覧回数
ctnxp
NXP Employee
NXP Employee

Hi Johnny, 


Our team is reviewing this and will get back to you soon. 

-Cynthia 

0 件の賞賛
返信