RAM usage on Kinetis Design Studio

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

RAM usage on Kinetis Design Studio

2,364 Views
miguelgonzalez
Contributor II

Hi everyone.

I'm using Thread protocol with a KW41Z kinetis. I'm trying to watch the RAM memory usage of one kinetis connected to the mesh but I can't. I would like to know how many memory a router is wasting when an end device sends a temperature string to the server.

Is there any way to watch the RAM memory usage  on the Kinetis Design Studio? Is there another way?

I'm using the example "router eligible device" of the SDK.

Thank you in advance.

0 Kudos
Reply
1 Reply

1,987 Views
gerardo_rodriguez
NXP Employee
NXP Employee

Hello Miguel,

The memory reserved for the temperature message is allocated by the memory manager. You can read more about the memory manager in chapter 3.3. Memory management the Connectivity Framework Reference Manual located in <Connectivity software path>\docs\wireless\Common\.

You can also analyze the RAM usage in the *.map file located in the Debug folder.

Regards,

Gerardo

0 Kudos
Reply