Hi, @Christine_Li
Thank you for your support.
I investigated the requested items and obtained the following results.
1. Reproduction on KW47-LOC
I tested the same software on a KW47-LOC board.
The issue is reproducible on the KW47-LOC as well.
HAL_RpmsgMcmgrInit() returns kStatus_HAL_RpmsgTimeout, and then the application reaches assert(false).
2. SDK Example Usage
The current project is not using an SDK example in its original form.
The software has been customized over time, and at this time I am unable to determine which SDK example, if any, was originally used as the project baseline.
Therefore, I cannot identify a specific SDK example that this project is based on.
3. Test with Software Reset
I also tested using Software Reset instead of Hardware Reset in IAR.
The same behavior occurs with Software Reset.
HAL_RpmsgMcmgrInit() returns kStatus_HAL_RpmsgTimeout, and then the application reaches assert(false).
4. Additional Information: NBU Version
I checked the NBU version using the API below:
int PLATFORM_GetNbuInfo(NbuInfo_t *nbu_info_p);
The returned values are:
- nbu_info->versionNumber[0] = 0x01
- nbu_info->versionNumber[1] = 0x09
- nbu_info->versionNumber[2] = 0x20
Based on these values, the reported NBU version appears to be 1.9.20.
Could you please confirm whether NBU version 1.9.20 is the expected and compatible version for SDK 26.03.00?
Please let me know if you need any additional information or logs.
BR,
hyama.