QN9090 - working with SDCARD

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

QN9090 - working with SDCARD

2,546 次查看
shai_b
Senior Contributor II

Hello Team,

My customer needs to implement SDCARD but he did not found any material to perform such SD card implementation with the QN9090 Dev kit.

please advise if there is an example code to add an SD card or can you guide us to implement an SD card?

second thing, the customer wanted to know if PWM output can be set to be a logical 1 of V-REF/BIAS/BAND GAP (for example if the PWM can be at peak 2.5v)? 

please advise back, Thanks in advance 

Kind regards,

Shai

标签 (1)
  • QN

标记 (2)
0 项奖励
回复
3 回复数

2,452 次查看
shai_b
Senior Contributor II

Hello team,

I did not hear from you for a while, I would really appreciate your support in #SDcard implementation with #QN9090 device.

Thanks in advance 

kind regards,

[email protected]‌

0 项奖励
回复

2,452 次查看
mario_castaneda
NXP TechSupport
NXP TechSupport

Hi Shai,

I hope you are doing great.

please advise if there is an example code to add an SD card or can you guide us to implement an SD card?

 Unfortunately, we do not provide any support with the SD Card. However, you could use the SPI or I2C example for a better reference for the customer implementation.

second thing, the customer wanted to know if PWM output can be set to be a logical 1 of V-REF/BIAS/BAND GAP (for example if the PWM can be at peak 2.5v)? 

The PWM output could be 2.5V depending on the VDDE. 

VDDE — Supply voltage for IO

pastedImage_2.png

Regards,

Mario

2,452 次查看
shai_b
Senior Contributor II

Mario,

Thank you.

0 项奖励
回复