QN9090 based consumer product FCC testing

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

QN9090 based consumer product FCC testing

2,025件の閲覧回数
alexedge
Contributor I

Hi,

I have a custom designed PCB and firmware using the QN9090. The only interface for programming during manufacturing is SWD and once inside a case can't be accessed. No UART available only a LCD display and single button. Is there a source code example of the types of operations required for FCC, such as transmitting on a certain channel. I believe there is a binary that can be used for FCC validation with the DK6 board but since my GPIO is very different and I don't have a UART available this won't work. I need to utilize the LCD and button to setup the various testing modes.

Thanks.

ラベル(1)
タグ(3)
0 件の賞賛
返信
1 返信

1,986件の閲覧回数
Ricardo_Zamora
NXP TechSupport
NXP TechSupport

Hi Alex,

 

Hope you are doing well. We have the QN9090 RF System Evaluation Report for BLE Applications (QN9090x_Certi_Tools.bi), but it needs a serial interface, I think this is the example you mentioned.

This example provides RF evaluation test results of the QN9090 for BLE applications (2FSK modulation).

You can download the MCUXpresso project from the QN9090 page:

Ricardo_Zamora_1-1653065494086.png

Hope this helps.

 

Regards,

Ricardo

0 件の賞賛
返信