QN908x and I2S

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

QN908x and I2S

794件の閲覧回数
carlobramini
Contributor II

Hello,

I'm evaluating the QN9080 mcu with the QN9080DK board and I'm wondering if this mcu is able to handle I2S communication.

By reading the UM11023 at page 272, paragraph "20.5 pin description" for the Flexcomm interface, and also in few other points of the manual, there are some references to it. But I have not found technical information for that.

In addition, the PSELID register does not seem to allow the selection of I2S RX/TX mode.

Could you give more information on that?

Thank you very much.

Sincerely.

タグ(2)
0 件の賞賛
返信
1 返信

676件の閲覧回数
gerardo_rodriguez
NXP Employee
NXP Employee

Hello Bramini,

Unfortunately, the QN908x does not support I2S. The references to I2S in the user manual are most probably a documentation error. I will report it to the corresponding team, so it gets fixed in future revisions of the user manual.

Thank you!

Best regards,

Gerardo

0 件の賞賛
返信