QN9080SIP

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

QN9080SIP

6,192件の閲覧回数
1758793535
Contributor I

Hi! Can you tell me where to set the server and client in the program?   Because there is only a client and no server on my device, the connection is always automatically disconnected. In the case of only client, how to set the connection?

thank you very much!

0 件の賞賛
返信
13 返答(返信)

6,184件の閲覧回数
nxf56274
NXP Employee
NXP Employee

Hi,

I am not sure what do you mean. The device can play the role as device and client.

The example 'wireless_uart' has the usage of this two role. If you still have the question, please describe it in detail such as which sdk and ide you use. 

Have a great day,
TIC

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 days after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 件の賞賛
返信

6,177件の閲覧回数
1758793535
Contributor I

Hello

  the situation is like this: I hope the development board Bluetooth can only be used as a server, because if the development board is used as a client, then my device(smartphone) needs a server, but there is no server on my device. This causes the connection to always be disconnected. So how can I modify the program to connect successfully?

thank you very much

0 件の賞賛
返信

6,174件の閲覧回数
nxf56274
NXP Employee
NXP Employee

Hi,

Except the wireless_uart, the example only plays role as client or server. They won't play as other role automatically. I am not sure why your device will change its own function.

Have a great day,
TIC

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 days after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 件の賞賛
返信

6,172件の閲覧回数
1758793535
Contributor I

hi

When establishing a connection, the development board will query whether my device has a client and a server. It must have both to successfully connect. If one of them is missing, it will automatically disconnect. Now my device has only client API but no server API, so I can't connect the development board.

thank you!

0 件の賞賛
返信

6,167件の閲覧回数
nxf56274
NXP Employee
NXP Employee

Hi,

Which example do you use? Which phone app do you use? The development board will query the device? what device?

Have a great day,
TIC

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 days after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 件の賞賛
返信

6,165件の閲覧回数
1758793535
Contributor I

HI

I use wireless_ uart。 I'm not using apps, I'm using web pages. It's just that the Bluetooth on the web page lacks the server API, which leads to the connection failure all the time.

thank you !

0 件の賞賛
返信

6,148件の閲覧回数
nxf56274
NXP Employee
NXP Employee

Hi,

I am not sure where you get the webpage. It looks like your webpage has some problem. The develoment board won't check if your webpage has the server or client. The board start broadcasting as server and your phone connect to it. After that, the phone request the server's characteristic. Then they can communicate. Have you used our iot tool box to test? http://d.firim.pro/fgx5

Have a great day,
TIC

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 days after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 件の賞賛
返信

6,145件の閲覧回数
1758793535
Contributor I

hi

Yes, I have tested it with IOT box. There is no problem with the development board. This is really a problem with the web page because it lacks the server API. So I want to ask how to connect with the development board when there is only client API on mobile phone or web page.

thank you!

0 件の賞賛
返信

6,138件の閲覧回数
nxf56274
NXP Employee
NXP Employee

Hi,

If the problem is on your webpage, sorry, I can't help you. I do not have the experience about the webpage programming.

Have a great day,
TIC

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 days after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 件の賞賛
返信

6,119件の閲覧回数
1758793535
Contributor I

hi

Excuse me, in wireless_uart_freertos , where is the program to connect the development board to the device?

thank you!

0 件の賞賛
返信

6,115件の閲覧回数
nxf56274
NXP Employee
NXP Employee

Hi,

If mcu is server. The host stack(invisible to us ) will inform the mcu using App_HandleHostMessageInput.

This function will call BleApp_ConnectionCallback.

Have a great day,
TIC

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 days after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 件の賞賛
返信

6,105件の閲覧回数
1758793535
Contributor I

~%7ABXE[}_$~K]1Z$O~@~1Y.pngHI,I want to set these pins to low level in the program. What should I do?

thank you!

0 件の賞賛
返信

6,134件の閲覧回数
1758793535
Contributor I

hi

Excuse me, I can modify the program of the development board to connect it with my web page (no server API)

thank you!

0 件の賞賛
返信