QN9021 failed to run BLE example project

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

QN9021 failed to run BLE example project

ソリューションへジャンプ
3,175件の閲覧回数
229856331
Contributor I

I run the prj_bass project, but it can not work.

I debug it with jlink, found that BLE stack APIs locate at the address around 0x01000000~0x0102000 (defined in  fw_func_addr.h), but the content of the chip in the range is all 0xFF.

SDK version 1.4.0

The marking letter of chip is  "9021    355Y5   00UMF"

I use the macro QN_9020_B4

ラベル(1)
  • QN

タグ(2)
0 件の賞賛
返信
1 解決策
3,055件の閲覧回数
mario_castaneda
NXP TechSupport
NXP TechSupport

Hi,

What is the example that you are trying to run?

What are the lib that you have included?

Please look at the next AN https://www.nxp.com/docs/en/application-note/AN12288.pdf 

Is it your custom board?

Regards,

Mario

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
3,056件の閲覧回数
mario_castaneda
NXP TechSupport
NXP TechSupport

Hi,

What is the example that you are trying to run?

What are the lib that you have included?

Please look at the next AN https://www.nxp.com/docs/en/application-note/AN12288.pdf 

Is it your custom board?

Regards,

Mario

0 件の賞賛
返信
3,055件の閲覧回数
229856331
Contributor I

Thanks!

The example is  QN902x_SDK_1.4.0\Projects\BLE\prj_bass.

I use the jlink commad in PRJROOT\src\link\iar\qn9020_flash.mac to get that the chip is “Device: QN9020 B3”.

After using the macro CFG_QN9020_B2, it works.

qn9020_flash.mac:

execUserReset()
{
__var chip_id;

chip_id = __readMemory32(0x40000088, "Memory");

if(chip_id == 0x2801) // QN9020 B0
{
__message "Device: QN9020 B0";
cfg_fw_9020_B0();
}
else if(chip_id == 0x2901) // QN9020 B1
{
__message "Device: QN9020 B1";
cfg_fw_9020_B1();
}
else if(chip_id == 0x2A01) // QN9020 B2
{
__message "Device: QN9020 B2";
cfg_fw_9020_B2();
}
else if(chip_id == 0x2B01) // QN9020 B3
{
__message "Device: QN9020 B3";
cfg_fw_9020_B2();
}
else if(chip_id == 0x2C01) // QN9020 B4
{
__message "Device: QN9020 B4";
cfg_fw_9020_B4();
}
else
{
__message "Error: unknown device ID: ", chip_id;
}
}

0 件の賞賛
返信