Porting Thread stack onto linux-wpan?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Porting Thread stack onto linux-wpan?

Jump to solution
4,456 Views
xinyu_chen
NXP Employee
NXP Employee

Is it possible to port the thread stack (can be use space) onto the linux-wpan? As we know the linux-wpan now support 802.15.4 MAC and 6lowpan support in the network stack level, if we can port the Thread stack onto it running on like 6UL/ULL with a external RF (e.g. MCR20A), it would be a perfect solution for a rich gateway, even with other wireless solutions integated like BLE/WIFI.

Thanks.

Labels (2)
0 Kudos
Reply
1 Solution
4,017 Views
xueliu
Contributor II
0 Kudos
Reply
3 Replies
4,018 Views
xueliu
Contributor II

Here is my MCR20A driver for Linux. https://github.com/xueliu/mcr20a-linux

0 Kudos
Reply
4,017 Views
xinyu_chen
NXP Employee
NXP Employee

Excellent!

What test have been done?

0 Kudos
Reply
4,017 Views
xueliu
Contributor II

Hello,

I have the same idea. Now I am working on the Linux driver for MCR20A. I will make it public when the basic functions are finished.

Regards,

Xue Liu

0 Kudos
Reply