Hi
I'm working on an NFC application that uses PN5190 and IMX 7 as a Host uC. I want to use the Secure Firmware Update feature provided by the GUI to upgrade the firmware for PN5190.
The feature works perfectly on the PNEV5190B dev kit which has K82 as a Host uC. Ideally, I want to find the UcBalFW used for the K82 in the dev kit and port it to IMX 7. However, it seems the latest UCBalFW source code supporting PN5190 (NxpNfcCockpit_VCOM_UcBalFW_v03.09.00) doesn't support/provide interfaces for the Secure Firmware Update.
Do you have or know where to find an example source code that I need?
Thanks,
Tuan