PNEV5190 BOM

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 
4,273件の閲覧回数
AgentSam
Contributor I

Hello,

Looking at the PNEV5190 BOM, I can only see "AgilePN". How can I get actual part numbers?
Particularly, I need to know the manufacturer's PN corresponding to AgilePN 180-78936 used on PNEV5190MB.

Thanks,

0 件の賞賛
返信
1 解決策
4,254件の閲覧回数
vicentegomez
NXP TechSupport
NXP TechSupport
. 1 CADPart 180-78936 IND PWR 160nH@100MHZ 930mA 2% 0805 2 L1, L3
Replacement LQW2BANR16G00L   MURATA    

Regards

 

元の投稿で解決策を見る

6 返答(返信)
4,168件の閲覧回数
jr_hernandez
Contributor II

Sorry, but still not a full BOM. I found the BOM for the Module board inside the pdf, but not for the base board.

0 件の賞賛
返信
4,189件の閲覧回数
jr_hernandez
Contributor II

Hi Vicente,

Full BOM file with comercial part numbers of all componentes inside the board is required as reference for our design.

Can you please procide such a file?

Regards, Ramon.

0 件の賞賛
返信
4,178件の閲覧回数
vicentegomez
NXP TechSupport
NXP TechSupport

on the next link, you can download several documents

https://www.nxp.com/webapp/Download?colCode=SW6594&appType=license

please check this one

TRD-X-PNEV5190M_B

 

regards

 

0 件の賞賛
返信
4,211件の閲覧回数
jr_hernandez
Contributor II

I can not find any solution. There is no full BOM anywhere, right?

0 件の賞賛
返信
4,224件の閲覧回数
jr_hernandez
Contributor II

HI, 

Same problem here with several components.

Can you please provide a BOM with part numbers accessible to us. I can not find AgilePN anywhere.

Regards, Ramon.

4,255件の閲覧回数
vicentegomez
NXP TechSupport
NXP TechSupport
. 1 CADPart 180-78936 IND PWR 160nH@100MHZ 930mA 2% 0805 2 L1, L3
Replacement LQW2BANR16G00L   MURATA    

Regards