PN5190 Cockpit Load secondary Firmware FAIL

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

PN5190 Cockpit Load secondary Firmware FAIL

1,223 Views
Arrey
Contributor I

We have one question need support.

 After using NFC Cockpit (version v7.4.0) to start the PNEV5190BP #PNEV5190BP,  use  the Extra TAB to Load Secondary Firmware, for Refresh the latest version Firmware.  NFC Cockpit automatically directs to the default folder. then start loading the firmware. But some error occured in the process, as shown in the figure. We have try many times but nothing else.

  We want test EMVCo PCD L1 test cases, but failed.

  What should we do in next?c9b353a8c04d571b3f8371d61dcdee3.png

 

0 Kudos
Reply
1 Reply

1,165 Views
danielchen
NXP TechSupport
NXP TechSupport

Hi @Arrey 

 

There are some description about loading secondary firmware in UG10025.   section 4.13

danielchen_0-1709607288037.png

 

https://www.nxp.com/docs/en/user-guide/UG10025.pdf

 

You also can try this function with the latest version of cockpit, v8.0

 

Regards

Daniel

0 Kudos
Reply