PDM: Unexpected call back Code 3 Number 61698

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

PDM: Unexpected call back Code 3 Number 61698

1,636件の閲覧回数
xubovey
Contributor III

hi,

thanks

i get the err log in the function, and most time it work well,

the log was:

err:

[07:41:38.180] PDM: Unexpected call back Code 3 Number 61698

[07:41:38.272] PDM: Unexpected call back Code 3 Number 61700

[07:41:38.272] PDM: Unexpected call back Code 3 Number 61697

[07:41:38.293] PDM: Unexpected call back Code 3 Number 61699

[07:41:38.311] PDM: Unexpected call back Code 3 Number 61697

[07:41:38.320] PDM: Unexpected call back Code 3 Number 61699

right:

[07:41:34.183] NodeNum: 0, NwkAddr: 0x9cc8, IeeeAddr:00158d000211ff3b.

[07:41:34.190] NodeNum: 1, NwkAddr: 0xfffe, IeeeAddr:0000000000000000.

the code was:

PUBLIC uint8 app_u8MacAddrAndIeeeAddrPrint(void)
{
uint16 u16DstAddr;
uint16 nodeNum = 0;

do
{
u16DstAddr = ZPS_u16AplZdoLookupAddr(ZPS_u64NwkNibGetMappedIeeeAddr(ZPS_pvAplZdoGetNwkHandle(),nodeNum));
DBG_vPrintf(TRACE_APP, "NodeNum: %d, NwkAddr: 0x%04x, IeeeAddr:%016llx.\n",
nodeNum,
u16DstAddr,
ZPS_u64NwkNibGetMappedIeeeAddr(ZPS_pvAplZdoGetNwkHandle(),nodeNum));
nodeNum ++;
}while (0xFFFE != u16DstAddr);

return nodeNum;
}

what should i do to fix the bug, thanks for your help!

ラベル(3)
タグ(2)
0 件の賞賛
返信
1 返信

1,558件の閲覧回数
mario_castaneda
NXP TechSupport
NXP TechSupport

Hi Xu,

I am not sure what is the values that you want.

Did you look at the appZpsExtendedDebug.c file?

C:\NXP\bstudio_nxp\sdk\JN-SW-4170\Components\ZigbeeCommon\Source\appZpsExtendedDebug.c

Regards,

Mario

0 件の賞賛
返信