NVT2006

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

NVT2006

2,062 Views
sudarshankr
Contributor I

Hi,

In my current design i am planning to use NVT2006 to do the Level translation between

1. 1.2V to 1.8V

2. 1.5V to 1.8V. 

Max operating speed is for SPI around 10MHz. Are there any concerns in this regard. 

Regards,

Sudarshan

0 Kudos
Reply
3 Replies

1,992 Views
sudarshankr
Contributor I

Hi Tomas,

Sorry for replying late as i didnot get the alert. 

Thanks for your feedback. In data sheet there is table which shows the PU's to be used b/w 1.5V to 1.8V . Am i missing something here? Please clarify

sudarshankr_2-1690443326851.png

 

 

Regards,

Sudarshan

 

 

0 Kudos
Reply

1,979 Views
TomasVaverka
NXP TechSupport
NXP TechSupport

Hi Sudarshan,

The tables you are referring to are inaccurate. The NVT2006 is about 14 years old IC and I do not know who designed this part and created these pull up tables. We will need to correct them in the datasheet, but it will take some time.

Best regards,

Tomas

0 Kudos
Reply

2,048 Views
TomasVaverka
NXP TechSupport
NXP TechSupport

Hi Sudarshan,

1. OK

2. I am afraid this will not work properly. The minimum voltage difference between the VCC(B) and VCC(A) is 0.6V.

BR, Tomas

0 Kudos
Reply