NO Bluetooth connection once again!!

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

NO Bluetooth connection once again!!

16,662 Views
ralphxyz
Contributor III

Rapid-IoT:

Yesterday I was at least getting prompted for a password now a P6E9D devic eis seen

but I do not get prompted for a password connection string.

Seems like someone programed this device and should be able to answer, most of the 

answers I have seen have been guesses " try 999999" or the like.

IMG_20190424_153441542.jpg

IMG_20190424_153426138.jpg

Thanks,

Ralph

Labels (1)
28 Replies

3,698 Views
mario_castaneda
NXP TechSupport
NXP TechSupport

Hi Ralph,

Could you please remove the device that you have added in the session in the rapid IoT?

pastedImage_1.png

Then could you please reset the rapid IoT with the default firmware that it has by default?

I want to confirm these steps. You could connect with the set up in the Phone, I recommend use the NXP application because is filtering other devices and you will find your device easily.

Let me know your findings.

Regards,

Mario

0 Kudos
Reply

3,698 Views
ralphxyz
Contributor III

I have been following the Rapid IoT Prototyping Tool User’s Guide!

I removed the device from the Hexiwear Docking station and now I make a bluetooth connection after doing the Provisioning. The sensors are sensing different sensings if I cover up the device the light sensor changes!

Using the hexiwear docking station I have a USB connection, I see a Laplink drive!

Ralph

0 Kudos
Reply

3,698 Views
mario_castaneda
NXP TechSupport
NXP TechSupport

Hi Ralph,

Please let me know if you still have issues with the rapid IoT.

Regards,

Mario

0 Kudos
Reply

3,698 Views
ralphxyz
Contributor III

YES, occasionally the NXP Rapid IoT will run after a hard reset, but only

after a hard reset and then occasionally.

Again occasionally using the Hexiwear docking station I will get a USB

connection showing a DAPLINK drive.

Is the DAPLINK drive the correct drive to use for reflashing?

Ralph

On Sat, May 18, 2019 at 9:10 PM mario_castaneda <[email protected]>

0 Kudos
Reply

3,698 Views
mario_castaneda
NXP TechSupport
NXP TechSupport

Hi Ralph,

Is the DAPLINK drive the correct drive to use for reflashing?

Yes, it is correct.

Regards,

Mario

0 Kudos
Reply

3,698 Views
ralphxyz
Contributor III

Thanks, I only occasionally see it but maybe the next time I will try to

reflash the device, it shouldn't hurt and "might" actually correct things.

Ralph

On Mon, May 20, 2019 at 5:04 PM mario_castaneda <[email protected]>

3,698 Views
ralphxyz
Contributor III

Done!!

Same result, after a reset the device never connects unless it is in the

docking station with a soft reset, then the bluetooth icon flashes for a

couple of minutes and the the sensor results are displayed but they are

static they do not change with changes to its environment. The bluetooth

icon never flashes again.

No other apps see the device (NXP Iot Toolbox, Weather Station).

Ralph

On Mon, May 13, 2019 at 4:47 PM mario_castaneda <[email protected]>

0 Kudos
Reply

3,698 Views
ralphxyz
Contributor III

If I turn Bluetooth off and on and reset I see P6E9D on the device list!!

BUT I do not have a password!! With Android there is no "ignore device". I have tried no password and 999999999, 99999999, 9999999, 999999, 99999 nothing works! 

Ralph

0 Kudos
Reply