NFC Mobile Device Tag detection using PN7150

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

NFC Mobile Device Tag detection using PN7150

2,342件の閲覧回数
Electronics_Engineer
Contributor I

Hi

I'm wondering that how can we identify the physical NFC Passive tag from the NFC Mobile device with Card Emulation Mode( Mobile Active NFC Tag i.e. Bill payment )??

0 件の賞賛
返信
3 返答(返信)

2,330件の閲覧回数
fangfang
NXP TechSupport
NXP TechSupport

Hello,

The customer can refer to NXP-NCI MCUXpresso example project as the below:

NXP-NCI MCUXpresso example Project

And find the application note of example as the link.

https://www.nxp.com/docs/en/application-note/AN11990.pdf.

There is the care emulation demo for PN7150 as the example. 

Have a nice day.

 

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-----------------------------------------------------------------------------

0 件の賞賛
返信

2,290件の閲覧回数
Electronics_Engineer
Contributor I

Hi @fangfang 

This document gives an example to use PN7150 as a card Emulation and an Android device as a reader.

I want the Android device to be in card emulation mode and PN7150 to identify Android Emulated card

Thanks

0 件の賞賛
返信

2,280件の閲覧回数
fangfang
NXP TechSupport
NXP TechSupport

Hello,

Please kindly follow  the guidelines as the link for your application.

URL:https://www.nxp.com/docs/en/application-note/AN11690.pdf.

 

Have a nice day.

 

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-----------------------------------------------------------------------------

0 件の賞賛
返信