NCJ29D5 error code 0XF2

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

NCJ29D5 error code 0XF2

1,407件の閲覧回数
longfeiwang
Contributor III

The anchor point ranging period is configured as 192ms. No matter whether the ranging is successful or not, the 29D5 will spit out a frame of RANGE_CCC_DATA_NTF at an interval of 192ms. However, when receiving air interference, the 29D5 will spit out RANGE_CCC_DATA_NTF slowly, and in many cases it will spit out once every 3s, and the distance cannot be measured within 3s. What is the reason for this situation? 

0 件の賞賛
返信
0 返答(返信)