Missing C++ guards and missing closing braces

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Missing C++ guards and missing closing braces

416 次查看
dstevens
Contributor II

This is a combination bug report / update request. The JN5189DK SDK (2.6.15) seems to have been at least partially written with C++ support in mind, as there are C++ include guards in many headers. Many others are missing though, and some of those that include C++ guards erroneously miss the closing statement.

For example, in `wireless/framework/Common/dbg.h`, the guard opens at top of file and closes inside a conditional block (#if (!defined JENNIC_CHIP_FAMILY_JN518x)). The conditional else block has no closing statement

#if defined __cplusplus
extern "C" {
#endif

#if (!defined JENNIC_CHIP_FAMILY_JN518x)
...
#if defined __cplusplus
};
#endif

#else /* JENNIC_CHIP_FAMILY is JN518x */
...
#endif

 

We are successfully building C++ applications, but the volume of changes required to add all of the guards makes migrating SDKs painful. Below is a non-exhaustive list of the errors and missing guards:

1. Missing closing braces:

- middleware/wireless/zigbee/ZigbeeCommon/Include/appZpsBeaconHandler.h
- middleware/wireless/framework/RNG/Interface/rnd_pub.h
- middleware/wireless/zigbee/ZCL/Clusters/OTA/Include/OTA.h


2. Completely missing guard

- middleware/wireless/zigbee/ZigbeeCommon/Include/ZQueue.h
- middleware/wireless/zigbee/ZigbeeCommon/Include/ZTimer.h
- middleware/wireless/zigbee/ZPSAPL/Include/zps_apl_zdo.h
- middleware/wireless/zigbee/ZPSAPL/Include/zps_apl_af.h
- middleware/wireless/zigbee/ZPSAPL/Include/zps_apl_aib.h
- middleware/wireless/zigbee/ZPSAPL/Include/zps_apl_zdp.h
- middleware/wireless/zigbee/framework/PDUM/Include/pdum_apl.h
- middleware/wireless/zigbee/ZCL/Clusters/General/Include/Scenes.h
- middleware/wireless/zigbee/ZCL/Clusters/General/Include/OnOff.h
- middleware/wireless/zigbee/ZCL/Clusters/General/Include/Groups.h
- middleware/wireless/zigbee/ZCL/Clusters/General/Include/MultistateInputBasic.h
- middleware/wireless/zigbee/ZCL/Clusters/General/Include/Identify.h
- middleware/wireless/zigbee/ZCL/Clusters/General/Include/Basic.h
- middleware/wireless/zigbee/ZigbeeCommon/Include/portmacro_JN518x.h (probably also 517x, 516x)


Code generation and others

- startup_JN5189.c: This file needs to be compiled as c++ to trigger the __libc_init_array call, but ResetISR2 needs C linkage in this case.

Additionally:
- pdum_gen.h - no include guard
- zps_gen.h - no include guard

There are likely many others. This is just those that we needed to modify to get our code compiling as C++.

Thanks for taking a look.

标记 (2)
0 项奖励
回复
1 回复

388 次查看
sofiaurueta
NXP Employee
NXP Employee

Hello,

 

Thank you for your feedback, I will check this internally with the responsible team.

 

Regards,

Ana Sofia.

0 项奖励
回复