MTBF Data for BGA3023Y

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

MTBF Data for BGA3023Y

5,093 次查看
harshithram
Contributor II

Hi,

We are using BGA3023Y-1.2GHz 20dB Gain CATV Amplifier in our design. What is the MTBF/Failure rate of that device?

Regards,

Harshith

2 回复数

5,005 次查看
vicentegomez
NXP TechSupport
NXP TechSupport

Hi 

The BGA3023 is no longer manufacturer and the MTBF is no longer available, all the information about this part is obsolete

BGA3023 Product Information|NXP 

Regards

4,999 次查看
harshithram
Contributor II

Thanks Vicente !

--

Regards,

Harshith

From: vicentegomez <[email protected]>

Sent: Wednesday, May 13, 2020 3:49 AM

To: Harshithram KV <[email protected]>

Subject: Re: - Re: MTBF Data for BGA3023Y

NXP Community

<https://community.freescale.com/resources/statics/1000/35400-NXP-Community-Email-banner-600x75.jpg>

Re: MTBF Data for BGA3023Y

reply from Vicente Gomez Salazar

<https://community.nxp.com/people/vicentegomez?et=watches.email.thread>

in *Wireless

Connectivity* - View the full discussion

<https://community.nxp.com/message/1310884?commentID=1310884&et=watches.email.thread#comment-1310884>

0 项奖励
回复