MMZ09332BT1

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MMZ09332BT1

1,871 Views
bsky2345
Contributor I

I want to use the MMZ09332BT1 in the frequency range 760-870 MHz, but with FR4 instead of RO4350B. I will change the trace width in the RF out and RF lines to achieve an impedance of 50 ohms. Should I consider anything else, such as the length of the VCC line?If the component was perfectly internally matched, I would make this change (using FR4) with confidence. However, the MMZ09332BT1 data sheet says that it "requires minimal external matching."

0 Kudos
Reply
2 Replies

1,771 Views
bsky2345
Contributor I

Hello

This tips help me and I redesign my pcb and sent for production.

Thanks

0 Kudos
Reply

1,847 Views
ErikaC
NXP TechSupport
NXP TechSupport

Hello, 

Substrate dielectric permittivity and thickness is critical. The width input/output traces is set to provide 50 Ohm impedance.

Datasheet specifies substrate RO4350B, Dk=3.66, the thickness is 10mil top dielectric layer. Three dielectric layers with total thickness of 32 mils.

Typical FR-4 has Dk=4.8. You can use the same layout as in the datasheet but the top dielectric layer thickness should be 12.3 mils (small variations possible, 12mils).

Hope this helps.

0 Kudos
Reply