MKW24D512 RF issue

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

MKW24D512 RF issue

2,186 次查看
haimliberman
Contributor I

Hi,

 

We have two setups (Coordinator + 16 routers and coordinator + 12 routers). All of the devices are using MKW24D512 processors.

 

We observed that ZigBee modules on coordinators stopped RF transmission on both networks after continuous operation of 40+ (43 and 44) days. In order to debug the issue, we used UART and we were able to communicate with the processor through ZTC command and read MAC address etc. This indicates that core of MKW24D512 processor was up and running and only RF part was having issues.

 

The solution we found to resolve the issue is to reset the ZigBee processor on coordinator, which is not desirable.

标签 (3)
标记 (1)
0 项奖励
回复
1 回复

1,999 次查看
stephanie_m
NXP TechSupport
NXP TechSupport

Hello, 

We no longer support/recommend BeeKit, but it is available for KW24D. 

Currently, the available devices with ZigBee support are the JN516x family and the KW41Z   

The currently supported stacks by KW24D are: Thread, 802.15.4 MAC and SMAC.

 

Regards, 

Estephania 

0 项奖励
回复