MKW24D512 RF issue

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

MKW24D512 RF issue

2,190件の閲覧回数
haimliberman
Contributor I

Hi,

 

We have two setups (Coordinator + 16 routers and coordinator + 12 routers). All of the devices are using MKW24D512 processors.

 

We observed that ZigBee modules on coordinators stopped RF transmission on both networks after continuous operation of 40+ (43 and 44) days. In order to debug the issue, we used UART and we were able to communicate with the processor through ZTC command and read MAC address etc. This indicates that core of MKW24D512 processor was up and running and only RF part was having issues.

 

The solution we found to resolve the issue is to reset the ZigBee processor on coordinator, which is not desirable.

ラベル(3)
タグ(1)
0 件の賞賛
返信
1 返信

2,003件の閲覧回数
stephanie_m
NXP TechSupport
NXP TechSupport

Hello, 

We no longer support/recommend BeeKit, but it is available for KW24D. 

Currently, the available devices with ZigBee support are the JN516x family and the KW41Z   

The currently supported stacks by KW24D are: Thread, 802.15.4 MAC and SMAC.

 

Regards, 

Estephania 

0 件の賞賛
返信