MKW22D and MKW24D difference

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

MKW22D and MKW24D difference

3,500 次查看
bimal
Contributor III

Hi,

I wanted to know the difeerences between MKW22D and MKW24D,

As it seems like both are pin compatible, both has equal Flash and RAM. Is there any major difference between them?

标签 (3)
0 项奖励
回复
3 回复数

3,033 次查看
EarlOrlando
Senior Contributor II

Hello Bimalsinh,

The differences are listed in the table 2.1 "Ordering Information" in the MKW2xD Reference Manual​.

kw.jpg

Best regards,

Earl.

3,033 次查看
bimal
Contributor III

Hi Earl,

Thanks for your feedback,

It seems like MKW24 supports Smart Energy 2.0, where as MKW22 doesn't. I am assuming that is the difference between them, otherwise they are same in Hardware architecture with pin-compatible.

I have one other question that, Does smart energy 2.0 requires any specific Hardware feature(like hardware stack support, IP stack) which is not there in MKW22?

0 项奖励
回复

3,033 次查看
jc_pacheco
NXP Employee
NXP Employee

SE2.0 relies on the SW stack, no hardware dependency. Only supported on MKW24.

0 项奖励
回复