MKW22 Footprint

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 
3,737件の閲覧回数
joelk
Contributor II

For the 8x8 MAPLGA foortpint should I include NC pads for the factory test pins 57-61 on the copper layer of my PCB as shown in the recommended footprint? or can they be omitted from the footprint all together?

Capture.JPG

0 件の賞賛
返信
1 解決策
3,602件の閲覧回数
AngelC
Senior Contributor I

Hello Joel,

You could leave pins 57-62 disconnected. Our actual development boards do not use those pins either; they are only used for factory test. You could however leave them in the layout for mechanical strength purposes as done in our evaluation boards. Just notice Pin 63 should be connected to ground as described in reference manual (PA supply ground).

Moreover, if you would like to see the TWR or USB KW2x boards schematics and layout, you may download them from our website for free. They might help you in your custom boards’ design process.

Regards,

AngelC

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
3,603件の閲覧回数
AngelC
Senior Contributor I

Hello Joel,

You could leave pins 57-62 disconnected. Our actual development boards do not use those pins either; they are only used for factory test. You could however leave them in the layout for mechanical strength purposes as done in our evaluation boards. Just notice Pin 63 should be connected to ground as described in reference manual (PA supply ground).

Moreover, if you would like to see the TWR or USB KW2x boards schematics and layout, you may download them from our website for free. They might help you in your custom boards’ design process.

Regards,

AngelC

0 件の賞賛
返信
3,602件の閲覧回数
joelk
Contributor II

Thanks!

0 件の賞賛
返信