MF DESFire EV 1 Update Binary

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

MF DESFire EV 1 Update Binary

3,342 次查看
zafer2021
Contributor I

Hi,

I am trying to write data to MF DESFire EV 1 card over RF, but I am having a problem. When I send update binary command I am getting 6700 wrong length error. Here is update binary command;

03 00 D6 00 02 05 54 02 65 6E 31

Could anyone help me?

0 项奖励
回复
1 回复

3,307 次查看
Kan_Li
NXP TechSupport
NXP TechSupport

Hi @zafer2021 ,

 

Mifare Desfire EV1 command information is available in the data sheet , but not allowed to discuss here as it is under NDA. You may request from the NXP doc store with a valid NDA. Please kindly refer to the attachment for more details.

 

Have a great day,
Kan


-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 项奖励
回复