MCUXpresso build code size

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

MCUXpresso build code size

3,322件の閲覧回数
seanwu
Contributor V

Dear sir,

I tried to build KW41 SDK example "frdmkw41z_wireless_examples_bluetooth_ble_fsci_black_box_freertos" using MCUXpresso, and the real code size is 242KB. But if I built binary file, the code size is 510KB. I checked the binary file, found MCUXpresso filled in "00" and "FF" after 3AD91. How to set MCUXpresso to build binary file code size  to 242KB without "00" and "FF" after 3AD91?

Thanks.

BR,

Sean

seanwu_0-1628124632165.png

seanwu_1-1628124741744.png

seanwu_2-1628124910426.png

 

 

ラベル(3)
0 件の賞賛
返信
2 返答(返信)

3,286件の閲覧回数
seanwu
Contributor V

Thank your sir.

0 件の賞賛
返信

3,291件の閲覧回数
Ricardo_Zamora
NXP TechSupport
NXP TechSupport

Hi Sean,

 

Hope you are doing well. The binary files generated by MCUXpresso for the KW41Z (specifically, for BLE projects and examples) are always the full 510kB in size, as to overwrite the whole PROGRAM_FLASH memory region, even filling the unused space with a "0xFF" value.

This is done on purpose, so old code is not left behind in unused memory regions of the PROGRAM_FLASH.

Hope this helps.

 

Best Regards,

Ricardo

0 件の賞賛
返信