MC13224

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MC13224

3,488 Views
reyz
Contributor I

Dear Manager,

While the part number branded on the Freescale label is SC667264, the part marking is showing MC13224. Is this SC667264 part number costumize to specific application or is it fully qualified or directly compatible with MC13224? is there any functional difference between the two part number?

0 Kudos
Reply
1 Reply

3,339 Views
karel_povalac
NXP Employee
NXP Employee

Hello,

thank you for interest about our products.

This specific part number (SC667264) can be used for our internal purposes. These chips can be used for the specific customer. However, the most important is the part number MC13224V. Which customer are you?

Thank's

Karel

0 Kudos
Reply