LX2160XE72232B-SFP+ Interfacing

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

LX2160XE72232B-SFP+ Interfacing

2,505件の閲覧回数
amrutha
Contributor I

Hi Team, we are using LX2160XE72232B NPU in our design .We have 10G SFP+ module in our design with connector UE76-A20-3000T. Is there any inbuilt coupling effect in the LX2160 side or Do we need to use extra coupling capacitors in TX and RX path in this interface ?

0 件の賞賛
返信
4 返答(返信)

2,468件の閲覧回数
JosephAtNXP
NXP TechSupport
NXP TechSupport

Hi,

That coupling effect is not built-in.

The reference design board has 0.47 uF capacitors coupling the SFP Phy connection and they have 20% tolerance.

Best regards, Joseph Linares

0 件の賞賛
返信

2,464件の閲覧回数
amrutha
Contributor I

Hi , is it ok if we give a provision with 0 ohm resistor ?

 

0 件の賞賛
返信

2,444件の閲覧回数
JosephAtNXP
NXP TechSupport
NXP TechSupport

I would recommend to stick with the capacitors that the reference design provided because I haven't met results replacing capacitors

Thank you!

0 件の賞賛
返信

2,478件の閲覧回数
amrutha
Contributor I

Hi Team,

Please help us with the prefered value ,tolerance , and placement of the  coupling capacitors that we should provide?

It would be helpful if you can provide the data  asap since we are in the critical stage of our project.

0 件の賞賛
返信