Hi @nxf77486 ,
We are working on an custom board, but we could now reproduce the failure also with the EVK.
If we run the digital key car anchor project on EVK and shortcut Y1 (R40) to GND than the BLE advertisement stops and does not recover once the shortage is removed. We are using SDK_2_12_7 and kw45b41_nbu_ble_1_9_12_3 for NBU.
If you don’t shortcut the 32MHz XTAL the BLE does not fail as often.
- Yes the connection stays stable. Only during ESD and Vehicle testing we can observe that sometimes the BLE functionality get's lost. If we run it "static" the failure did not occurred over months. That's why we are now checking how the system reacts on failures.