KW41Z for ZigBee

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

KW41Z for ZigBee

Jump to solution
14,037 Views
sensenthuran
Contributor IV

Is there any way to use KW41Z by loading ZigBee application (instead of using  JN series - JN5168)?

As we don't have space to keep both KW & JN series chipsets, we are planning to use KE41Z with BLE & Thread. If we need Zigbee, we should be able to switch to that by loading the stack.

Thanks 

Tags (3)
1 Solution
12,122 Views
jc_pacheco
NXP Employee
NXP Employee

ZigBee will not be supported on KW41Z. MKW41Z Connectivity Software covers: BLE, Thread, GENFSK, IEEE802.15.4 and SMAC.

Update: ZigBee 3.0 will be supported in KW41Z in Q1 2018.

View solution in original post

14 Replies
12,122 Views
jc_pacheco
NXP Employee
NXP Employee

Hello Mark, 

It's been recently decided to provide ZigBee support also on KW41Z. This is currently under development.

PartKey FeaturesCPUMemory
Flash/RAM
Frequency bandSupported ProtocolsRX SensitivityTX PwrRX currentTX current
KW40ZBLE & IEEE802.15.4Cortex-M0+160KB/20KB2.4 GHzBLE, Thread (End Device), 802.15.4 MAC, SMAC -96 dBm (BLE)
 -102 dBm (802.15.4)
Up to
+5 dBm
6.5 mA8.4 mA
KW30ZBLECortex-M0+160KB/20KB2.4 GHzBLE -91 dBmUp to
+5 dBm
6.5 mA8.4 mA
KW20ZIEEE802.15.4Cortex-M0+160KB/20KB2.4 GHzThread (End Device), 802.15.4 MAC, SMAC -102 dBmUp to
+5 dBm
6.5 mA8.4 mA
KW41ZBLE & IEEE802.15.4Cortex-M0+256-512KB/64-128KB2.4 GHzBLE, Thread, ZigBee Pro, 802.15.4 MAC, SMAC -96 dBm (BLE)
 -102 dBm (802.15.4)
Up to
+4 dBm
6.2 mA6.0 mA
KW31ZBLECortex-M0+256-512KB/64-128KB2.4 GHzBLE -96 dBmUp to
+4 dBm
6.2 mA6.0 mA
KW21ZIEEE802.15.4Cortex-M0+256-512KB/64-128KB2.4 GHzThread, ZigBee Pro, 802.15.4 MAC, SMAC -102 dBmUp to
+4 dBm
6.2 mA6.0 mA
KW2xDIEEE802.15.4Cortex-M4256-512KB/32-64KB2.4 GHzThread, ZigBee Pro, 802.15.4 MAC, SMAC -120 dBmUp to
+8 dBm
19.5 mA18 mA

Regards,

JC

0 Kudos
Reply
12,122 Views
senizhuseyin
Contributor I

Hello Juan,

We are starting a project in which we plan to use KW41Z. Is it certain that Zigbee Stack will be available in MKW41Z. If yes, when will the next MKW41Z with Zigbee stack is planned to be released?

Regards,

Seniz

0 Kudos
Reply
12,122 Views
jc_pacheco
NXP Employee
NXP Employee

Hello Seniz, 

ZigBee stack for KW41Z is planned to be fully released in Q1 2018.

-JC

0 Kudos
Reply
12,122 Views
markwinston
Contributor I

Thanks but I'm not sure you really answered my question.  Where can I find a list of what protocols are supported TODAY on your chips.  The table you sent is helpful, but if I understand correctly, it is inaccurate as it list that the KW41Z supports zigbee, while today it really doesn't have a zigbee stack availible, which is what i'm interested.  I'm thinking that it might be most efficient to just talk to someone at NXP on the phone rather than going back and forth on a thread.  Do you have a recommendation on what would be the best number to call to get this type of information, and what times would be best to call?

0 Kudos
Reply
12,122 Views
dominikertl
Contributor I

Will only the Zigbee stack not supported by nxp or Zigbee as technology in general for the KW41Z?

-> in another link on the Web the KW41Z is promoted with possibility for Zigbee: Freescale Kinetis KW41Z Wireless MCU Supports Bluetooth 4.2, Zigbee, and Thread 

and on the NXP page they say:

ARM Cortex-M0+|Kinetis KW41Z 2.4 GHz 32-bit MCUs|NXP 

"KW41Z is an ideal solution for true single chip designs that require concurrent communication on both a Bluetooth low energy network and an 802.15.4 based network such as Thread." -> here SUCH AS is the keyword for me

-> For example, would it be possible to use another 3rd party stack from e.g., Ubis*s (http://www.ubisys.de/en/engineering/products-c7b.html) ?

0 Kudos
Reply
12,124 Views
jc_pacheco
NXP Employee
NXP Employee

Hello Dominik, 

ZigBee stack will not be supported in KW41Z, only on JNxx devices.

The link that mentions ZigBee on KW41Z is not up-to-date (Oct 2015).

The SUCH AS, refers to the fact that there are multiple custom-stacks based on IEEE802.15.4 and we also provide the IEEE802.15.4 and SMAC standalone stacks which enable customers to generate their own stack/solution or work on the Thread Stack that is already provided.

12,124 Views
markwinston
Contributor I

Hi Juan,

I feel like I am missing something.  I feel like I've read tons of stuff that suggest this chip supports zigbee (i.e. but support I mean NXP provides zigbee stack and application profiles).  But it sounds like you are saying that is not true.

Do you know where can I get a full list of Stacks and app profiles that are supported for this chip (and the MKW-40).  I'm in the process of creating a trade study table that lists all NXP SoCs that have hardware and software (stacks and apps) support for BLE, Zigbee, and Thread.  My table will also list all the pertinent specs also, including cost.  However, I'd hope this would already be available from NXP rather than me having to learn this by reading forums.  Do you know where I can find at least a list of the protocols/stacks supported for a particular SoC?  

For example: I'm also trying to figure out if there is a thread stack for the MKW-40?  The datahsheet suggest that it exists, but the Connectivity Software didn't seem to have anything for Thread.

Thanks for the help.  I've spent the last view days reviewing all the details of this chip, so sort of let down now that I find out it can't do zigbee.  

Mark

0 Kudos
Reply
12,123 Views
jc_pacheco
NXP Employee
NXP Employee

ZigBee will not be supported on KW41Z. MKW41Z Connectivity Software covers: BLE, Thread, GENFSK, IEEE802.15.4 and SMAC.

Update: ZigBee 3.0 will be supported in KW41Z in Q1 2018.

12,124 Views
alexwheeler
Contributor I

Is it supported yet?  

0 Kudos
Reply
12,124 Views
jc_pacheco
NXP Employee
NXP Employee

Hi Alex, it's currently planned for the end of March. I'll keep you posted.

0 Kudos
Reply
12,124 Views
alexwheeler
Contributor I

Thanks for your reply. You helped me before with a Thread issue.

Will it support ZLL?

0 Kudos
Reply
12,124 Views
jc_pacheco
NXP Employee
NXP Employee

Hi Alex,

Update: There are additional tests being executed on the stack. ZigBee release will be ready until April 2018.

Yes, ZLL will be supported as part of ZigBee 3.0.

0 Kudos
Reply
11,538 Views
TommyTom
Contributor I

Hi,

So, is there a ZigBee stack available for the KW41Z? More specifically, for the USB-KW41Z. I have been searching for it and I simply cannot find it. Thank you.

0 Kudos
Reply
12,124 Views
alexwheeler
Contributor I

Thanks for the update.

0 Kudos
Reply