KW41Z LPUART

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

KW41Z LPUART

1,833件の閲覧回数
jricaurtepino
Contributor II

Hi

I´m developing a project that works with the MCU KW41Z on MCUXpresso IDE. 

I´m new at MCUXpresso (i used to work on Kinetis Design Studio with other microcontroler: kl27z256). at KDS, i used to work with processor expert, and had all the libreries for lpuart comunication.

On MCUXpresso, i understand that for mi microcontroler (KW41Z), I cant use the peripheral config tool .

im trying with the fsl_lpuart.h library, but its not working.

Could anyone tell me the best way to implement lpuart comunications in my project.

 

Thanks 

Jose

0 件の賞賛
返信
1 返信

1,809件の閲覧回数
nxf56274
NXP Employee
NXP Employee

Hi,

You can use the example. Click 'import SDK examples'. Choose your board. Then you can import the 

lpuart example.

 

22.PNG

33.PNG

 

Have a great day,
TIC

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 days after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------