KW36 reading flash data caused HardFault_Handler

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

KW36 reading flash data caused HardFault_Handler

2,943件の閲覧回数
wjw2026
Contributor II

Hi:

KW36 reading flash data caused HardFault_Handler!


1、different data is written to the same flash address twice consecutively。

uint8_t wdata[8] = {0x11,0x22,0x33,0x44,0x55,0x66,0x77,0x88};
NV_FlashProgram(0x00073778, 8, wdata);
wdata[0] = 0x00;
NV_FlashProgram(0x00073778, 8, wdata);

2、reading flash data caused HardFault_Handler。

uint8_t rdata[8] = {0};
memcpy(rdata, 0x00073778, 8);

3、The ecc verification error may occur because data is written to the same address twice;How does this error not trigger HardFault_Handler; can trigger FTFE_IRQHandler !

0 件の賞賛
返信
5 返答(返信)

2,923件の閲覧回数
Ricardo_Zamora
NXP TechSupport
NXP TechSupport

Hello,

 

Hope you are doing well. Could you please clarify what SDK version are you using?

 

Are you using an SDK example as a base? What modifications did you make?

 

Are you using a FRDM?

 

Why are you writing different data on the same address consecutively?

 

Regards,

Ricardo

0 件の賞賛
返信

2,892件の閲覧回数
wjw2026
Contributor II

sdk ver 2.25

Continuously write different data on the same address just to repeat the problem, the actual application does not know how to produce, the phenomenon is to read flash cause  HardFault_Handler.

NV FlashProgram for write and memcpy for read.

0 件の賞賛
返信

2,884件の閲覧回数
Ricardo_Zamora
NXP TechSupport
NXP TechSupport

Hello,

 

The recommended API's are located on <SDK_Path>\middleware\wireless\framework\Flash\Internal\. The main functions are:

NV_FlashEraseSector

NV_FlashProgram

NV_FlashRead (FLib_MemCpy)

 

Regards,

Ricardo

0 件の賞賛
返信

2,799件の閲覧回数
wjw2026
Contributor II

Hello,

      Hope to get your help!

0 件の賞賛
返信

2,873件の閲覧回数
wjw2026
Contributor II

My requirement is very simple, is to read flash exception when do not trigger HardFault_Handler, can trigger FTFE_IRQHandler, how to configure? 

0 件の賞賛
返信