KW01 Frequency setting?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

KW01 Frequency setting?

1,029件の閲覧回数
lucianomoretti
Contributor IV

I'm looking at the KW01 for use in Amature Radio.  The Amature radio frequency ranges are 420-450MHz and 902-928MHz.  The Fact sheet lists 424-510MHz and 862-1020MHz as supported by the KW01 which overlap fairly well with the amature bands but I'm having trouble figuring out how the frequency is set.  The MRB-KW01 board comes in three flavors for the 862-1020MHz bands, but doesn't list the exact ranges supported and I'm having trouble finding information on how to select the 424-510mhz range.

If someone could point me in the way of an App Note it would be appreciated.

タグ(3)
0 件の賞賛
返信
2 返答(返信)

857件の閲覧回数
mario_castaneda
NXP TechSupport
NXP TechSupport

Hi Luciano,

Pleas take a look for the next link;

How to configure KW01_IEEE_802_15_4 to operate on EU Frequency Band 

Let me know if you have problems with the frequency, hope it helps

Best Regards,

Mario

0 件の賞賛
返信

857件の閲覧回数
lucianomoretti
Contributor IV

So if I understand it correctly, it's completely determined in software?  Why have the 3 versions of the MRB-KW01 then?

0 件の賞賛
返信