K32W pins

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

K32W pins

2,385 Views
danieltseng
Contributor V

Refer to JN-AN-1242-Customer-Module-Eval-Tool.pdf

Where are the pins of DIO10 and DIO17?
I have searched for the carrier board and module board, but none of them on schematic.

pastedImage_1.png

pastedImage_2.png

Labels (1)
  • KW

1 Reply

2,310 Views
Sebastian_Del_Rio
NXP Employee
NXP Employee

Hi Daniel, I hope you're doing well!

 

Some documents use different nomenclature to refer to the same pins, for instance, DIO and PIO. These both refer to the same pin, which corresponds to the following functionality:

pastedImage_2.png

pastedImage_3.png

(taken from the part's datasheet)

 

And are routed to connector J3 in the OM15076 Carrier Board:

pastedImage_7.png

(taken from the Design Files package, which you can find in the Product Page for the Development Kit)

 

Please let me know if you need any more information.

 

Best regards,

Sebastian