K32W pins

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

K32W pins

2,373件の閲覧回数
danieltseng
Contributor V

Refer to JN-AN-1242-Customer-Module-Eval-Tool.pdf

Where are the pins of DIO10 and DIO17?
I have searched for the carrier board and module board, but none of them on schematic.

pastedImage_1.png

pastedImage_2.png

ラベル(1)
  • KW

1 返信

2,298件の閲覧回数
Sebastian_Del_Rio
NXP Employee
NXP Employee

Hi Daniel, I hope you're doing well!

 

Some documents use different nomenclature to refer to the same pins, for instance, DIO and PIO. These both refer to the same pin, which corresponds to the following functionality:

pastedImage_2.png

pastedImage_3.png

(taken from the part's datasheet)

 

And are routed to connector J3 in the OM15076 Carrier Board:

pastedImage_7.png

(taken from the Design Files package, which you can find in the Product Page for the Development Kit)

 

Please let me know if you need any more information.

 

Best regards,

Sebastian