JN5189 send data

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

JN5189 send data

1,539 Views
Viki
Contributor II
Hi All, The chip I use is JN5189, and the SDK version I use is SDK2.6.2_JN5189. I developed based on the zigbee_coordinator,zigbee_router, and zigbee_ed_rx_off routines. I want to know how do I add the MAC address of the sender node to the packet when I broadcast, multicast, and unicast wireless data?(The default is the sender's network address) BR, Viki
0 Kudos
Reply
1 Reply

1,522 Views
nxf56274
NXP Employee
NXP Employee

Hi,

Please refer the 'JN-UG-3130-Zigbee3-Stack.pdf', chapter 5.5. It is in the directory 'JN5189DK6.zip\docs\wireless\Zigbee'

Have a great day,
TIC

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 days after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 Kudos
Reply