The SDK version of JN5189 is 2.6.4, and the jN-AN-1244 routine is 2005.
I have installed the add Cluster step to add this WWAH.
Is your WWAH function available?
The following error was reported when I compiled:
c:/nxp/mcuxpressoide_11.5.0_7232/ide/tools/bin/../lib/gcc/arm-none-eabi/10.3.1/../../../../arm-none-eabi/bin/ld.exe: ../../../Binaries/ExtendedColorLight_NtagIcode_GpCombo_Ota_OM15081/obj/WWAHCommandHandler.o: in function `eCLD_WWAHCommandHandler':
WWAHCommandHandler.c:(.text.eCLD_WWAHCommandHandler+0x9b4): undefined reference to `ZPS_u8AplExtdedAibGetWWAH'
c:/nxp/mcuxpressoide_11.5.0_7232/ide/tools/bin/../lib/gcc/arm-none-eabi/10.3.1/../../../../arm-none-eabi/bin/ld.exe: WWAHCommandHandler.c:(.text.eCLD_WWAHCommandHandler+0x9be): undefined reference to `ZPS_vAplExtdedAibSetWWAH'
c:/nxp/mcuxpressoide_11.5.0_7232/ide/tools/bin/../lib/gcc/arm-none-eabi/10.3.1/../../../../arm-none-eabi/bin/ld.exe: WWAHCommandHandler.c:(.text.eCLD_WWAHCommandHandler+0xa2c): undefined reference to `ZPS_u8AplExtdedAibGetWWAH'
c:/nxp/mcuxpressoide_11.5.0_7232/ide/tools/bin/../lib/gcc/arm-none-eabi/10.3.1/../../../../arm-none-eabi/bin/ld.exe: WWAHCommandHandler.c:(.text.eCLD_WWAHCommandHandler+0xa34): undefined reference to `ZPS_vAplExtdedAibSetWWAH'
c:/nxp/mcuxpressoide_11.5.0_7232/ide/tools/bin/../lib/gcc/arm-none-eabi/10.3.1/../../../../arm-none-eabi/bin/ld.exe: WWAHCommandHandler.c:(.text.eCLD_WWAHCommandHandler+0xa5a): undefined reference to `ZPS_u8AplExtdedAibGetWWAH'
c:/nxp/mcuxpressoide_11.5.0_7232/ide/tools/bin/../lib/gcc/arm-none-eabi/10.3.1/../../../../arm-none-eabi/bin/ld.exe: WWAHCommandHandler.c:(.text.eCLD_WWAHCommandHandler+0xa64): undefined reference to `ZPS_vAplExtdedAibSetWWAH'
collect2.exe: error: ld returned 1 exit status
make: *** [Makefile:688: ../../../Binaries/ExtendedColorLight_NtagIcode_GpCombo_Ota_OM15081/ExtendedColorLight_NtagIcode_GpCombo_Ota_OM15081.axf] Error 1
ad