JN5179 write attrib 0x10 to IASZone with 0xF0 data type fail

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

JN5179 write attrib 0x10 to IASZone with 0xF0 data type fail

1,667 Views
benjaminchang
Contributor V

With JN5179, we hope to perform enrolment to IASZone device. We take Device (JN-AN-1218-Zigbee-3-0-Light-Bulb-v1002,DimmableLight), and added IASzone cluster. Try on Coordinator (JN-AN-1216-Zigbee-3-0-IoT-ControlBridge) with ZGWUI tool, but failed.

We followed "Section 36 of JN-UG-3115", and try to accomplish "36.3.2  Auto-Enroll-Response". The 2nd item is "Write Attribute command" with IEEE address (8-byte). But "data" field of ZGWUI can accept single hex data only. Below are the logs. Please check and comment. Is there a way that we can accomplish the enrollment task using ZGWUI?

pastedImage_1.png

Raw Data/Received Message

<1>[Read Attrib] with (E_CLD_IASZONE_ATTR_ID_IAS_CIE_ADDRESS=0x0010)

09:28:16.189 -> 01 02 11 02 10 02 10 02 1E E6 02 12 6A 81 02 11 02 11 02 15 02 10 02 10 02 10 13 02 17 02 11 02 10 10 03

09:28:16.301 <- 01 80 00 00 04 83 00 06 01 00 03

09:28:16.371 <- 01 81 00 00 14 94 06 6A 81 01 05 00 00 10 00 F0 00 08 00 00 00 00 00 00 00 00 03

Type: 0x8000 (Status)

  Length: 4

  Status: 0x00 (Success)

  SQN: 0x06

  Message: _

Type: 0x8100 (Read Attrib Response)

  SQN: 0x06

  Src Addr: 0x6A81

  EndPoint: 0x01

  Status: 0x00

  Cluster ID: 0x0500 (Security & Safety: IAS Zone)

  Attribute ID: 0x0010

  Attribute Size: 0x0008

  Attribute Type: 0xF0 (IEEE Address)

  Attribute Data: 00:00:00:00:00:00:00:00 //(IEEE address after reset)

<2>[Write Attrib] with (Type:E_ZCL_IEEE_ADDR = 0xf0, Data=0x38 //1-byte, ZGWUI required(or err)

>Got: (Write Attrib Response) with error!

09:28:33.165 -> 01 02 11 10 02 10 10 20 02 12 6A 81 02 11 02 11 02 15 02 10 02 10 02 10 13 02 17 02 11 02 10 10 F0 38 03

09:28:33.309 <- 01 80 00 00 04 92 00 07 01 10 03

09:28:33.401 <- 01 81 10 00 0C 12 07 6A 81 01 05 00 7F 38 20 00 00 00 03

Type: 0x8000 (Status)

  Length: 4

  Status: 0x00 (Success)

  SQN: 0x07

  Message: __

Type: 0x8110 (Write Attrib Response)

  SQN: 0x07

  Src Addr: 0x6A81

  Src Ep: 0x01

  Cluster ID: 0x0500 (Security & Safety: IAS Zone)

  Attribute ID: 0x7F38                           // error why?

  Attribute Size: 0x0000                        // ??

  Attribute Type: 0x00 (Unknown)        // ??

  Status: 0x20                                        // ??

<3>[Read Attrib] with (E_CLD_IASZONE_ATTR_ID_IAS_CIE_ADDRESS=0x0010)

>got: Attribute Data: 38:38:38:38:38:38:38:38  // seems the 1st byte has been changed

09:28:40.796 -> 01 02 11 02 10 02 10 02 1E E6 02 12 6A 81 02 11 02 11 02 15 02 10 02 10 02 10 13 02 17 02 11 02 10 10 03

09:28:40.933 <- 01 80 00 00 04 8D 00 08 01 00 03

09:28:42.551 <- 01 81 00 00 14 9A 08 6A 81 01 05 00 00 10 00 F0 00 08 38 38 38 38 38 38 38 38 03

Type: 0x8000 (Status)

  Length: 4

  Status: 0x00 (Success)

  SQN: 0x08

  Message: _

Type: 0x8100 (Read Attrib Response)

  SQN: 0x08

  Src Addr: 0x6A81

  EndPoint: 0x01

  Status: 0x00

  Cluster ID: 0x0500 (Security & Safety: IAS Zone)

  Attribute ID: 0x0010

  Attribute Size: 0x0008

  Attribute Type: 0xF0 (IEEE Address)

  Attribute Data: 38:38:38:38:38:38:38:38      // seems the 1st byte has been changed

<4.TBD>[Write Attrib] with Data=00:15:8D :00:00:E0:7A:3E //8-byte,ZGWUI is to be revised

 Regards,

Benjamin

0 Kudos
Reply
2 Replies

1,417 Views
mario_castaneda
NXP TechSupport
NXP TechSupport

Hi Benjamin,

A local sales will be in touch with you for solve this issue.

Regards,

Mario

0 Kudos
Reply

1,417 Views
vivekvaghela
Contributor I

Hi Mario,

I am also having the same query. I am having one Door Sensor (IAS Zone Device). I want to enroll it using IEEE address of control bridge app (running on JN5179 USB dongle) by write attribute command from ZGWUI. But the tool is not allowing me to write 8 bytes. Can you please help me here to get the solution?

Thanks,

Vivek

0 Kudos
Reply