JN5169 uart is connected to linux

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

JN5169 uart is connected to linux

3,200件の閲覧回数
jaeoh
Contributor I

Hi,

I want to operate JN5169 on a embeded linux platform using uart directly.

So, a linux application commands scan, join, and others to this, and then controls it. 

But, some people said that it may be impossible becaue of some reasons.

For example, JN516x series do not support linux platform, and only operate on JenOS or RTOS, and so on.

Is it impossible?

Thanks.

ラベル(2)
0 件の賞賛
返信
3 返答(返信)

2,716件の閲覧回数
limcb
Contributor IV

Hi, please take a look at JN-AN-1216-Zigbee-3-0-IoT-ControlBridge-v1004

There should be a pdf under Doc. 

0 件の賞賛
返信

2,718件の閲覧回数
jaffinmk
Contributor III

Hi Lim

I had checked out the application that you had said but it includes only a TestGUI which runs on Windows. Also I like to implement light link profile so I checked the JN-AN-1223 ZigBee IoT Gateway Control Bridge from this link ZigBee Light Link|NXP .

But it doesnt give linux gateway implementation. I need to control my JN5168 bridge from linux.

0 件の賞賛
返信

2,716件の閲覧回数
limcb
Contributor IV

If you are developing a linux gateway, you should be looking at JN-AN-1222.

0 件の賞賛
返信