JN5169 Zig Bee / Thread - SSPark

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

JN5169 Zig Bee / Thread - SSPark

2,078件の閲覧回数
haydnyoon
NXP Employee
NXP Employee

About JN5169:

  1. How can I create a trust zone (security key storage, etc)?
    For example, is it automatically generated from chip vendor's stack?
    Is sample code provided and can be changed by customer?
  2. Can I support AES256 in Zigbee wireless communication?
  3. What are the features of AES256?
    For instance, device security, trust zone, fw update over the air.
  4. What is the difference between Zigbee 2.0 and Zigbee 3.0?
  5. Is zigbee 3.0 compatible with other vendor zigbee chip and NXP zigbee 2.0 device?
  6. How can I ensure compatibility with Zigbee 3.0?
  7. What are the differences between Zigbee 3.0 and the DotDot certification program?
  8. What are the features of Zigbee green power?
  9. Is there a way to avoid interference and collision in addition to CSMA/ CA and AN5158 in Zigbee?
  10.  What is the status of the NXP ZigBee Market in China and what are the major customers?
  11. Is the software ready to check the actual operation of Thread?
  12. Thread and ZigBee 3.0 (include DotDot) Interworking plan and recommand?


0 件の賞賛
返信
1 返信

1,948件の閲覧回数
stephanie_m
NXP TechSupport
NXP TechSupport

Hello,

How can I create a trust zone (security key storage, etc)? For example, is it automatically generated from chip vendor's stack? Is sample code provided and can be changed by customer?

What do you mean by trust zone ? Like in the ARM technology ?

Can I support AES256 in Zigbee wireless communication?

Key-based Encryption A very high-security, 128-bit AES-based encryption system (built into the JN516x/7x device as a hardware function) is applied to network communications, preventing external agents from interpreting ZigBee network data

What are the features of AES256? For instance, device security, trust zone, fw update over the air.

Well, AES256 it's an encryption algorithm so I'm not sure I understand your question.

What is the difference between Zigbee 2.0 and Zigbee 3.0?

Is zigbee 3.0 compatible with other vendor zigbee chip and NXP zigbee 2.0 device?How can I ensure compatibility with Zigbee 3.0?

 Could you please check this link ?

What are the differences between Zigbee 3.0 and the DotDot certification program?

Do you mean the differences between the certifications ?

What are the features of Zigbee green power?

Please, check these two links.

https://www.nxp.com/docs/en/user-guide/JN-UG-3119.pdf 

https://www.zigbee.org/zigbee-for-developers/greenpower/

What is the status of the NXP ZigBee Market in China and what are the major customers?

  As this it's confidential  information I do not believe we should share any of this in a public community that everyone can see such as this. Sorry for the inconvenience this might cause you.

Is the software ready to check the actual operation of Thread?

Thread it's currently only supported in the KW41Z

Thread and ZigBee 3.0 (include DotDot) Interworking plan and recommand?

Could you please help me with more details of what do you mean with this question?

Regards,

Estephania

0 件の賞賛
返信