JN 5168 Not rejoining network

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

JN 5168 Not rejoining network

3,185 Views
henrylavin
Contributor I

I have a jn5168 here.  If I provision it to a meter and then turn it on, the device works fine, usually.

However, if I turn the device off (unplug the device) it does not reconnect to the network upon reconnecting the power.

Also if I drop the device from the network, it does not re-scan for channels.

I think this is a problem with key establishment between the meter and the device, however I am not sure, does anyone know what is going on here.  Any help is welcome.

Thank you

3 Replies

2,779 Views
janibal
Contributor II

Hi, if the network is setup with security and you delete the network context when you start the device, this one won't rejoin. Check the "PDM_vDeleteAllDataRecords()" that delete the context, but you should be keep it.

0 Kudos
Reply

2,779 Views
ygensas
Contributor II

Hello,

I'm new also on JN5168 ZigBee module.

So I start with the SDK guide (ref. JN-UG-3064), and they talk about an template but impossible to download it (JN-AN-1158) => dead link.

Does someone know how to download it ?

Henry Lavin, you are try to connect your module, you should have the response ?

Best regards,

0 Kudos
Reply

2,779 Views
anikethesamudra
Contributor II

Hello Henry,

I am sorry that I am unable to answer your question. I am commenting here so that I could get some sort of help!

I am currently working on JN5168 ZigBee Module. I am new to the ZigBee Application Development. I am currently working on the Smart Energy SDK. (IPD Node and Energy Smart Meter) The contents are so much to go through. I want to learn based on some tutorials (step by step) to get better understanding. Could you please suggest me any tutorials or guides? I downloaded the application notes but I am getting lost because of huge content! I downloaded the application note IPD (In Premise Display - End Device) and ESP-EM (Energy Monitor - Master Device) onto the JN5168 module. But when I turn on, they are not getting connected. Could you please help me? I do not know where I am getting lost. It has lot of content that I do not know the starting point to work on.

Thanking you,

Best Regards,

Aniketh

0 Kudos
Reply