Is any console log output from UART if I download MAC 2006 FSCI 115200 KW41 ASP_RadioTest.srec into FRDM-KW41Z

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Is any console log output from UART if I download MAC 2006 FSCI 115200 KW41 ASP_RadioTest.srec into FRDM-KW41Z

1,848件の閲覧回数
Danube
Contributor IV

Hi Sir,

I can't see any console log from OPENSDA debug port if I download MAC 2006 FSCI 115200 KW41 ASP_RadioTest.srec into FRDM-KW41Z.

1 返信

1,469件の閲覧回数
karel_povalac
NXP Employee
NXP Employee

Hello Danube‌,

I tried to compile and load the MAC_FSCI_app for the FRDM-KW41Z. I sent the console commands through the NXP Test Tool 12. The board responded on the console. Please try to use it (load the MAC2006_g command set). The Test Tool will also decode particular commands.

Karel