Importing existing projects inKDS

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Importing existing projects inKDS

2,311 次查看
marbro1965
Contributor I

Hi,

I want to start a new project for R41Z evaluation kit and for this I import an existing project.

Is there any way to import a project and not to have linked files but their copy in my workspace?

Best Regards

0 项奖励
回复
3 回复数

2,176 次查看
jorge_a_vazquez
NXP Employee
NXP Employee

Hi marbro1965

If you are using MKW41Z_ConnSw_1.0.2, You can clone the example projects with project cloner tool. You should find it in the default path: C:\nxp\MKW41Z_ConnSw_1.0.2\tools\wireless\ProjectCloner


Hope this information helps you
Have a great day,
Jorge Alcala

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复

2,176 次查看
marbro1965
Contributor I

I exactly did this operaction but when i open the cloned project the files

are linked files,

not copies to work directory.

Regards

2017-01-23 19:31 GMT+01:00 jorge_a_vazquez <[email protected]>:

NXP Community

<https://community.freescale.com/resources/statics/1000/35400-NXP-Community-Email-banner-600x75.jpg>

Re: Importing existing projects inKDS

reply from Jorge Antonio Alcala Vazquez

<https://community.nxp.com/people/jorge_a_vazquez?et=watches.email.thread>

in Wireless Connectivity - View the full discussion

<https://community.nxp.com/message/870862?commentID=870862&et=watches.email.thread#comment-870862>

0 项奖励
回复

2,176 次查看
jorge_a_vazquez
NXP Employee
NXP Employee

Hi marbro1965

It will copy the files from wireless connectivity software and place it in your project, but at the moment to call them, these files are linked. You can modify them now, and your original files inside the connectivity software will not be affected (cause you have now copy).

Best Regards

Jorge Alcala

0 项奖励
回复