ISO14443 device level compatibility with MIFARE

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

ISO14443 device level compatibility with MIFARE

Jump to solution
2,114 Views
meekeech
Contributor I

I'm aware that there's a standard called ISO 14443 and an associated testing standard that is at a component level (ie PN7462 module).

My question is: if I'm designing a custom version of an existing evaluatoin board (ie PNEV7462C), do I need to test to the ISO standard mentioned for my new antenna size?

Is there a chance we won't successfully communicate with something like an Infineon tag or a MIFARE or something? 

 

Thank you,

MArko

0 Kudos
Reply
1 Solution
2,094 Views
Fabian_R
NXP TechSupport
NXP TechSupport

Thank you for your interest in our products.

ISO14443 is a standard for a type of RFID tag, It isn't required to work with it but, most of the tags that are sold work under it.

This will depend entirely on the tag you will communicate to.

In order to design an antenna please take a look at our Antenna Design Guide.

https://www.nxp.com/docs/en/application-note/AN11706.pdf

Best Regards,
Fabian

View solution in original post

0 Kudos
Reply
1 Reply
2,095 Views
Fabian_R
NXP TechSupport
NXP TechSupport

Thank you for your interest in our products.

ISO14443 is a standard for a type of RFID tag, It isn't required to work with it but, most of the tags that are sold work under it.

This will depend entirely on the tag you will communicate to.

In order to design an antenna please take a look at our Antenna Design Guide.

https://www.nxp.com/docs/en/application-note/AN11706.pdf

Best Regards,
Fabian
0 Kudos
Reply