I3C using FRDM-MCXW71 board

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

I3C using FRDM-MCXW71 board

Jump to solution
1,184 Views
compcorp
Contributor I

Hi there,

I'm wondering if it's possible to evaluate I3C using the FRDM-MCXW71 board.  Documentation for the board suggests that only I2C support is enabled, specifically for LPI2C1 peripheral.  Technically the MCU could be reconfigured to be I3C for those pins, (or alternatively the SPI could be reconfigured), but the traces on the board connect to the accelerometer and the MCU-Link, as well as the various IO Headers (Arduino etc).

What limitations would be encountered if I3C was configured on either of those ports? Would there be a preferred approach?

Best Regards

Ross 

0 Kudos
Reply
1 Solution
1,034 Views
compcorp
Contributor I

Thanks! I'll look into it.

View solution in original post

0 Kudos
Reply
2 Replies
1,035 Views
compcorp
Contributor I

Thanks! I'll look into it.

0 Kudos
Reply
1,124 Views
RomanVR
NXP Employee
NXP Employee

Hello @compcorp, hope you are doing well.

It is possible to use I3C with the FRDM-MCXW71, specifically on the J2 header in which pins 1 and 2 are routed to MCU pins which can be configured for I2C or I3C. For a reference example please refer to the SDK (v25.12.00 preferably) which includes board to board examples that may act as reference on how to configure the I3C module properly.

Please let me know if these work for you.

Best Regards!
0 Kudos
Reply