I used SMAC Codebase for MC1322x . I want PWM sample code in Generic Application code, Please help me.

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

I used SMAC Codebase for MC1322x . I want PWM sample code in Generic Application code, Please help me.

1,909件の閲覧回数
charnonpoolsin
Contributor I

I used SMAC Codebase for MC1322x . I want PWM sample code in Generic Application code, Please help me.

You may use 1322x Sensor Node board for this application.

Thanks you.

0 件の賞賛
返信
1 返信

1,741件の閲覧回数
AngelC
Senior Contributor I

Dear Charnon,

An easy and fast way to learn how to use the Timer module and the TMR drivers described in 22xDRVRRM is to check the BuzzerInit() function inside the Sound.c file of your project. The Buzzer configures the timer module to generate interrupts.

I am also sending you an example code I wrote some time ago using the SMAC Generic App. This code implements the TMR drivers of the MC1322x MCU and their basic functionality. The program starts a timer that toggles its output (PIN 1 in SRB) every 100 ms and enters a callback function every time the counter is reached (every 100 ms). Feel free to use it as an example for your implementation.

Please refer to the timer configuration example for fixed-frequency PWM mode of the timer mode included in the MC1322x Reference manual- chapter 12.7.11 Fixed-Frequency PWM Mode. There are many other configuration examples you may use too.

MC1322xRM: http://cache.freescale.com/files/rf_if/doc/ref_manual/MC1322xRM.pdf

Regards,

AngelC

0 件の賞賛
返信