How to get battery power ?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

How to get battery power ?

2,878件の閲覧回数
yaoxingshan
Contributor II

The development board I am using is FRDM-KW41Z.

Is there any API related to reading the power supply voltage in the SDK package?

Thank!

ラベル(2)
タグ(2)
0 件の賞賛
返信
2 返答(返信)

2,678件の閲覧回数
stephanie_m
NXP TechSupport
NXP TechSupport

Hello, 

Are you looking to use a specific protocol ? Are you looking to use Thread? 

You can check for example in the reed example the API called BOARD_GetBatteryLevel ? Does that work for you ? 

Regards, 

Estephania 

0 件の賞賛
返信

2,678件の閲覧回数
yaoxingshan
Contributor II

Hello there,

I am using a Thread Stack.

Does the API need to set the power mode to a specific mode?

I saw in the manual that the DCDC module needs to configure the registers to connect the DCDC module to the ADC channel, so do I need to write the registers separately?

Thank!

0 件の賞賛
返信