How to enable OTA Multicast option in NXP Test Tool?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

How to enable OTA Multicast option in NXP Test Tool?

3,206件の閲覧回数
joachimk
Contributor II

I'm using NXP Test Tool to Over-The-Air update the firmware of multiple target platforms (based on KW41z).

Updating a single module takes arround 5 minutes. But if a update 10 module at once, OTA time will increase to approx. 30 minutes!

In NXP Test Tool Software, there is a (greyed out!) checkbox for enabling OTA Multicast, which I can't set to active.

What can I do to enable OTA Multicast?

Are there some other performace optimizations I can do, to speed up OTA process?

ラベル(3)
2 返答(返信)

2,886件の閲覧回数
pavel_krenek
NXP Employee
NXP Employee

Hi Joachim,

regarding the multicast feature in the NXP Test Tool it is not free feature as Estephania mentioned you need to contact local sales team.

Best regards,

Pavel

2,886件の閲覧回数
stephanie_m
NXP TechSupport
NXP TechSupport

Hello,

To make the process faster you will either need to use multicast or update a smaller image. 

For more information on how to enable the multicast in the NXP Test Tool, please contact your local sales team.

If you have any other doubt, please let me know.

Regards,

Estephania

0 件の賞賛
返信